SNVSCT1 October 2025 LM5066H
ADVANCE INFORMATION
Refer to the PDF data sheet for device specific package drawings
LM5066H1 can be used with a VCL of 25 or 50mV using CL pin configurations (Connect CL pin to GND to set the nominal overcurrent threshold at 50mV. Connecting CL to VDD sets the overcurrent threshold to be 25mV). Using the DEVICE_SETUP2 (EFh, Read/Write Word) register, the current limit can be set at 10mV, 12.5mV, 15mV, 17.5mV, 20mV, and 22.5mV. TI recommends targeting a current limit that is at least 10% above the maximum load current to account for the tolerance of the LM5066H1 current limit. Targeting a current limit of 110A, the sense resistor can be computed as follows:
Typically, sense resistors are only available in discrete values. If a precise current limit is desired, a sense resistor along with a resistor divider can be used as shown in Figure 8-2.
Figure 8-2 SENSE Resistor DividerThe next larger available sense resistor should be chosen (250µΩ in this case). The ratio of R1 and R2 can be computed as follows:
Note that the SENSE pin pulls 25μA of current, which creates an offset across R2. TI recommends keeping R2 below 10Ω to reduce the offset that this introduces. In addition, the 1% resistors add to the current monitoring error. Finally, if the resistor divider approach is used, the user should compute the effective sense resistance (RSNS,EFF) using Equation 9 and use that in all equations instead of RSNS.

R1 is selected as 10Ω, R2 becomes 1.01Ω. Closest selected value of R2 is 1Ω.
Note that for many applications, a precise current limit may not be required. In that case, it is simpler to pick the next smaller available sense resistor.