SNVSBJ0B December 2019 – August 2021 LM5170
PRODUCTION DATA
TI recommends setting a hard limit of the maximum current programming signal such that the converter cannot be over driven by an errant current programming signal. Assume the converter is allowed up to 10% overloading current. Refer to Equation 7, the analog current setting signal ISETA must be limited by the following voltage level:

Refer to Equation 10, the PWM current setting signal ISETD must be limited by the following duty cycle: