SLVSIM2A June 2025 – August 2025 TPD4S480-Q1
PRODUCTION DATA
USB PD has a specification for the total amount of capacitance that is required for proper USB PD BMC operation on the CC lines.
| NAME | DESCRIPTION | MIN | MAX | UNIT | COMMENT |
|---|---|---|---|---|---|
| cReceiver | CC receiver capacitance | 200 | 600 | pF | The DFP or UFP system have capacitance within this range when not transmitting on the line |
When USB PD is in use, keep the capacitance of the CC lines between 200pF and 600pF. The combination of capacitances added to the system by the TPS2674x-Q1, the TPD4S480-Q1, and any external capacitor need to fall within these limits.