JAJSQP4 February 2024 ADS1288
PRODUCTION DATA
The modulator is an inherently stable design and, therefore exhibits predictable recovery from input overdrive. If the modulator is overdriven at the peaks of the input signal, the filter output data can clip, but not necessarily so depending on the duration of the signal overdrive resulting from data averaging of the digital filter. If the modulator is heavily overdriven, then the likelihood of clipped conversion data in the output increases. Be aware the group delay of the digital filter delays the time of an input overdrive event to the output data.