JAJSQ90 september 2020 TSB41BA3F-EP
PRODUCTION DATA
The S2_PC0, S1_PC1, and S0_PC2 terminals can be used in some port speed/mode selections to set the default value of the power-class indicated in the pwr field (bits 21–23) of the transmitted self-ID packet. Descriptions of the various power-classes are given in Table 13-9. The default power-class value is loaded following a hardware reset, but is overridden by any value subsequently loaded into the Pwr_Class field in register 4.
PC0–PC2 | DESCRIPTION |
---|---|
000 | Node does not need power and does not repeat power. |
001 | Node is self-powered and provides a minimum of 15 W to the bus. |
010 | Node is self-powered and provides a minimum of 30 W to the bus. |
011 | Node is self-powered and provides a minimum of 45 W to the bus. |
100 | Node can be powered from the bus and is using up to 3 W; no additional power is needed to enable the link. The node can also provide power to the bus. The amount of bus power that it provides can be found in the configuration ROM. |
101 | Reserved for future standardization. |
110 | Node is powered from the bus and uses up to 3 W. An additional 3 W is needed to enable the link. |
111 | Node is powered from the bus and uses up to 3 W. An additional 7 W is needed to enable the link. |