SFFS983 August 2025 MSPM0G1518 , MSPM0G1519 , MSPM0G3518 , MSPM0G3519
Package pin-related failures are covered by one or more of the safety mechanisms described. There are two different types of pins.
In the case of GPIO pins, depending on the signal chosen in the context of the application, the safety mechanism applicable to the corresponding IP covers the pin failures. For cases where the pins are reset or power pins, the safety mechanisms covering reset or power are used. For more information, refer to the safety analysis report.