SFFS983 August 2025 MSPM0G1518 , MSPM0G1519 , MSPM0G3518 , MSPM0G3519
In this test method, the GPIO pin is setup with a known value and the status of the pin can be read back using the DIN register. The loopback happens at the I/O driver, and hence, can read the pin status. This method can be applied when the GPIO is configured as an output.