SLAAEO4 November 2025 MSPM0G3507 , MSPM0L1306
For the device to support ROM or Flash BSL, the 256-bit BSL access password is always enabled. There are two types of password for MSPM0. The first type is a 256-bit plain text password, with the default of an 0xFF value. As Section 4.3 shows, the second type is SHA2-256 encrypted, the original password is all 0xFF (256-bit), so that the SysConfig tool stores the generated SHA2-256 value of the original password into the PWDBSL.PASSWORD field.