SLAAEO4 November 2025 MSPM0G3507 , MSPM0L1306
If the NONMAIN configuration disables the SWD interface or locks the debug access, send the BSL command to unlock the device after BSL mode entry.
BSL Communication Interface (see Section 3.2.3) is applied to send BSL command. The ROM BSL core supports the Factory Reset command to restore the default NONMAIN configurations. Refer to MSPM0 Bootloader user's guide for more details.
The approach is not viable in the following situations: