SLAAEO4 November 2025 MSPM0G3507 , MSPM0L1306
For the devices support ROM or Flash BSL, TI provides access ability to the device memory through the BSL interface. One default BSL invoke pin is used for hardware invoking BSL, see Section 3.2.2 for more details.
User can disable BSL through the BOOTCFG2.BSLMODE field, which fully disables BSL mode. The BSL software invoke (through the SYSRST) is also blocked.
Alternatively, disable BSL invoke pin check using the BOOTCFG1.BSL_PIN_INVOKE field blocks the BSL hardware entry. After disable the invoke pin check, the device does not check the invoke pin status during the boot, so that the BSL hardware entry is disabled. Users can enter the BSL using software invoke method in the application code.