In addition to the provided equipment
detailed in section Section 1.2, the following equipment
is not included with the EVM kit, but is required for proper evaluation.
- TSW14J58EVM FPGA Capture card for
capturing data from the ADC, and everything required for operation according to the
TSW14J58EVM User’s Guide TSW14J58EVM.
- High-Speed Data Converter Pro Software
(HSDC Pro) High Speed Data Converter Pro
- GSPS FPGA SERVER GSPS
FPGA SERVER download link
- One 12 Volt power supply capable of
supplying 5Amps
- At least two low-noise signal generators
to provide the ADC sampling clock and analog inputs to the ADC. TI recommends either of
the following signal generators:
- Rohde and Schwarz SMA100A
- Rohde and Schwarz SMA100B
- A lower performance signal generator is also required as a reference clock to the
ADC:
- This clock does not affect ADC performance and is only be used for
functionality.
- Bandpass filters for the sample clock and
analog inputs. It is recommended to use filters with a narrow passband (within 5%-15% of
the desired bandwidth), and minimal insertion loss.
- SMA cables to connect the inputs
By default, the EVM is configured for an
external reference clock to be provided, there are optional board modifications that can be
done to allow for only a single clock be supplied to the ADC EVM. These modifications are
noted in Section 5.2