SPRAD20 March 2022 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
At initialization, outputs of software resolver are passed to global variables with pointers as shown in the following line 1 and 2. As motor angle is always changing during rotation, it will not be meaningful if it is not plotted in graph window at a fixed sample frequency. Line 3 and line 4 pass the addresses of resolver angle and speed to two log pointers. They are logged every assigned number of interrupts by the log functions described in Section 2.4.3.