SPRAD67D September 2024 – October 2025 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The processor families support up to x5 (five) concurrent external Ethernet ports. Pinmuxing overlaps for one of the CPSW3G0 and PRU1_ICSSG instances.
For more information, refer the application note Five-Ethernet-Port Enablement on AM64x and AM243x.
The processor families support three MDIO interfaces and the recommendation is to connect CPSW3G0 MDIO to CPSW3G0 Ethernet ports, PRG0 MDIO port to ICSSG0 Ethernet ports, and the PRG1 MDIO port to ICSSG1 Ethernet ports.
Before using the Ethernet ports and configuring the MDIO interface (for boot and normal operation), refer to advisory i2329 MDIO: MDIO interface corruption (CPSW and PRU-ICSS) in the AM64x/AM243x Processor Silicon Revision 1.0, 2.0.
For more information on the Ethernet interface, see the following FAQs:
[FAQ] AM625 / AM623 / AM620-Q1 / AM625-Q1 / AM625SIP: Ethernet PHY RGMII synchronous clock
The FAQ is generic and can also be used for AM64x and AM243x processor families.