SPRAD67D September 2024 – October 2025 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
When selecting crystal for MCU_OSC0, the recommendation is to consider the temperature and aging characteristics based on the worst case operating environment and expected life expectancy of the custom board or the end equipment. Verify the crystal load and the crystal load capacitor value used (including addition of the PCB capacitance (for MCU_OSC0)) matches the device-specific data sheet recommendations. The recommendation is to select crystal load which allows selection of a standard capacitor value. Mismatch in value can introduce clock frequency PPM errors.
For more information, see the following FAQ:
For more information, see the MCU_OSC0 Crystal Circuit Requirements table of the device-specific data sheet.
The recommendation is to connect the MCU_OSC0 crystal directly to the processor as per device-specific data sheet.
The recommendation is to verify the crystal selection with the crystal manufacturer (as required).