SPRAD67D September 2024 – October 2025 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
In case the project is to design a new board or platform, the recommendation is to use the latest Version/Revision of the software development tools.
AM64x Processor Family:
Refer below link to download the required SDK version:
PROCESSOR-SDK-LINUX-AM64X: Processor SDK Linux for AM64x
PROCESSOR-SDK-LINUX-AM64X-HS: Processor SDK Linux for AM64 HS
MCU-PLUS-SDK-AM64X: MCU+ SDK for AM64x – RTOS, No-RTOS
Refer to AM64x Software Build Sheet (Build Sheet of supported features for AM64x processor family).
In case an older Version/Revision is being used, the recommendation is to verify the compatibility using the release notes or reach out to TI (through E2E).
AM243x Processor Family:
Refer below link to download the required SDK version:
MCU-PLUS-SDK-AM243X: MCU+ SDK for AM243x – RTOS, No-RTOS
In case an older Version/Revision is being used, the recommendation is to verify the compatibility using the release notes or reach out to TI (through E2E).