SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Table 11-51 lists the memory-mapped registers for the EMIF1_CONFIG_REGS registers. All register offset addresses not listed in Table 11-51 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Write Protection | Section |
|---|---|---|---|---|
| 0h | EMIF1LOCK | EMIF1 Config Lock Register | EALLOW | Go |
| 2h | EMIF1COMMIT | EMIF1 Config Lock Commit Register | EALLOW | Go |
| 4h | EMIF1MSEL | EMIF1 Controller Sel Register | EALLOW | Go |
| 8h | EMIF1ACCPROT0 | EMIF1 Config Register 0 | EALLOW | Go |
Complex bit access types are encoded to fit into small table cells. Table 11-52 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| R-0 | R -0 | Read Returns 0s |
| Write Type | ||
| W | W | Write |
| WSonce | W Sonce | Write Set once |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
| Register Array Variables | ||
| i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
| y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. | |
EMIF1LOCK is shown in Figure 11-38 and described in Table 11-53.
Return to the Summary Table.
EMIF1 Config Lock Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | LOCK_EMIF1 | ||||||
| R-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-1 | RESERVED | R | 0h | Reserved |
| 0 | LOCK_EMIF1 | R/W | 0h | Locks the write to access protection and controller select fields for EMIF1: 0: Write to ACCPROT and MSEL fields are allowed. 1: Write to ACCPROT and MSEL fields are blocked. Reset type: SYSRSn |
EMIF1COMMIT is shown in Figure 11-39 and described in Table 11-54.
Return to the Summary Table.
EMIF1 Config Lock Commit Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | COMMIT_EMIF1 | ||||||
| R-0h | R/WSonce-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-1 | RESERVED | R | 0h | Reserved |
| 0 | COMMIT_EMIF1 | R/WSonce | 0h | Permanently Locks the write to access protection and controller select fields for EMIF1: 0: Write to ACCPROT and MSEL fields are allowed based on value of lock field in EMIF1LOCK register. 1: Write to ACCPROT and MSEL fields are permanently blocked. Reset type: SYSRSn |
EMIF1MSEL is shown in Figure 11-40 and described in Table 11-55.
Return to the Summary Table.
EMIF1 Controller Sel Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| KEY | |||||||
| R-0/W-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| KEY | |||||||
| R-0/W-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| KEY | |||||||
| R-0/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| KEY | RESERVED | MSEL_EMIF1 | |||||
| R-0/W-0h | R-0h | R/W-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | KEY | R-0/W | 0h | Writing the value 0x93A5CE7 will allow the writing of the EMIF1MSEL bits, else writes are ignored. Reads will return 0. Reset type: CPU1.SYSRSn |
| 3-2 | RESERVED | R | 0h | Reserved |
| 1-0 | MSEL_EMIF1 | R/W | 0h | Controller Select for EMIF1: 00: CPU1 is controller but not grabbed. CPU2 can grab the controller ownership by changing this value to '10'. 01: CPU1 is controller. 10: CPU2 is controller. 11: CPU1 is controller but not grabbed. CPU2 can grab the controller ownership by changing this value to '10'. Reset type: CPU1.SYSRSn |
EMIF1ACCPROT0 is shown in Figure 11-41 and described in Table 11-56.
Return to the Summary Table.
EMIF1 Config Register 0
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | DMAWRPROT_EMIF1 | CPUWRPROT_EMIF1 | FETCHPROT_EMIF1 | ||||
| R-0h | R/W-0h | R/W-0h | R/W-0h | ||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-3 | RESERVED | R | 0h | Reserved |
| 2 | DMAWRPROT_EMIF1 | R/W | 0h | DMA WR Protection For EMIF1: 0: CPU Writes are allowed. 1: CPU Writes are blocked. Reset type: SYSRSn |
| 1 | CPUWRPROT_EMIF1 | R/W | 0h | CPU WR Protection For EMIF1: 0: CPU Writes are allowed. 1: CPU Writes are blocked. Reset type: SYSRSn |
| 0 | FETCHPROT_EMIF1 | R/W | 0h | Fetch Protection For EMIF1: 0: CPU Fetches are allowed. 1: CPU Fetches are blocked. Reset type: SYSRSn |