SPRUJ17I March 2022 – August 2025 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
In this mode, the I2C module is a target and receives data from a controller. All targets begin in this mode. Serial data bits received on the SDA pin are shifted in with the clock pulses that are generated by the controller device. The target device does not generate the clock, but it can hold the SCL pin low while intervention of the device is required (RSFULL = 1) after a byte has been received.