SPRUJH0B April 2025 – September 2025
The F28E12x LaunchPad has several power domains that can be connected or isolated from each other with removable shunts. The different 3.3V and 5V power domains are further described in Figure 2-2.
| Shunt Identifier | Usage Description |
|---|---|
| JP1, +5V0 | Connects the +5V power from the USB-C connector (+5V0_USB) to the +5-V power on the XDS side of the board (+5V0_XDS110). Bridges the power isolation between the USB and XDS planes. |
| JP1, GND | Connects the board Ground on the isolated USB-C connector side of the board (USB_GND) to the rest of the board ground (GND). Bridges the ground isolation between the USB side and the rest of the board. |
|
JP2, +5V0 |
Connects the +5-V power from the XDS side of the board (+5V0_XDS110) to the +5-V power on the MCU side of the board (+5V0_MCU). |
|
JP2, +3V3 |
Connects the +3.3-V power from the XDS side of the board (+3V3_XDS110) to the +3.3-V power on the MCU side of the board (+3V3_MCU). |
| J17 | Enables the onboard 3.3V to 5V BOOST regulator to convert the +3.3V power rail to a +5V power rail. |
The F28E12x LaunchPad features a flexible power domain scheme that allows users to supply power to the board in a variety of different configurations. Table 2-2 shows the different power configurations and the required shunts that need to be populated to supply power throughout the board.
| Power Source | Connected Shunts | Description of Power Sources |
|---|---|---|
| USB-C Connector | JP1, JP2 |
+5V0_USB: supplied from the USB-C connector +5V0_XDS110: +5V0_USB passes through JP1 and is the same supply as +5V0_XDS110 +5V0_MCU: +5V0_XDS110 passes through JP2 and is the same supply as +5V0_MCU +3V3_XDS110: generated by the XDS-side 5V to 3.3V LDO regulator +3V3_MCU: +3V3_XDS110 passes through JP2 and is the same supply as +3V3_MCU |
| External +3.3-V (connected to BoosterPack header) | JP2 +5V0 (optional), J17 |
+5V0_USB: If debugging the device, then connect JP2 +5V0 shunt to provide power to the XDS110 debugger. +5V0_USB is supplied through the USB-C connector and is isolated from the MCU side +5V0 rail. Else if not debugging, +5V0_USB is not required and JP2 +5V0 can be disconnected +5V0_XDS110: Required only if debugging the device. +5V0_MCU passes through JP2 and is the same supply as +5V0_XDS110 +5V0_MCU: generated by the 3.3V to 5V BOOST regulator +3V3_XDS110: Required only if debugging the device. +3V3_XDS110 is generated by the XDS-side 5V to 3.3V LDO regulator. Make sure JP2 +3V3 shunt is disconnected to prevent contention on the 3.3V power rail +3V3_MCU: supplied by external +3.3V source |
| External +5.0-V (connected to BoosterPack header) |
JP2 |
+5V0_USB: If debugging the device, +5V0_USB is supplied through the USB-C connector and is isolated from the MCU side +5V0 rail. Else if not debugging, +5V0_USB is not required. +5V0_XDS110: 5V0_XDS110 passes through JP2 and is the same supply as +5V0_MCU +5V0_MCU: supplied by external +5.0V source +3V3_XDS110: +3V3_XDS110 passes through JP2 and is the same supply as +3V3_MCU +3V3_MCU: generated by the XDS-side 5V to 3.3V LDO regulator |