SBASAI9 December 2025 ADS112S14 , ADS122S14
PRODUCTION DATA
Figure 9-5 and Figure 9-6 show the measurement results for a 4-wire Pt100. The measurements are taken at TA = 25°C using precision resistors instead of a 4-wire Pt100. Figure 9-5 shows both the resistance measurement error without any calibration and after a system offset and gain calibration. The respective temperature measurement error in Figure 9-6 is calculated from the offset and gain error corrected data in Figure 9-5 using the NIST tables.
The design meets the required temperature measurement accuracy given in the Design Requirements. However, the measurement error shown in Figure 9-6 does not include the error of the RTD.