SBASAX4 June 2026 ADS9316 , ADS9317
PRODUCTION DATA
In default operation, the ADS931x initiates the conversion on the falling edge of CONVST. The device offers the ability to invert CONVST so that the device initiates the ADC conversion on the rising edge of CONVST. To enable this mode, write 1b to CONVST_INVERT in address 0x14. Figure 6-21 illustrates the timing when CONVST is inverted. If low latency mode is enabled, verify that tph_CV is greater than tCONV + tLOW_LAT, so that the ADC output is from the current ADC sample.