SBAU487 August 2025
To use the ADS131M08MET-EVM, two pieces of software must be installed on the PC being used to evaluate the EVM. If using the USB to RS-232 cable provided with the EVM, the drivers for the cable must be installed. Download the U209-000-R cable drivers from the EATON serial adapter cable link.
The second piece of software needed is the MSPM0-SDK. The SDK package includes the CCS project file that is used to create the firmware loaded into the MSPM0G1506 as well as the Energy Metrology GUI.