SBAU487 August 2025
For the following test results, gain and phase calibration are applied to the EVM using CR8350-2500-N current transformers from CR Magnetics Inc. In the following results, the active energy results are within 0.1% at 0° phase shift. Additionally, the active energy versus voltage results and the RMS voltage results show that good accuracy results are able to be obtained despite using only a fraction of the ADC range for the voltage channels.
The % Error columns in the following tables and plots are calculated as the difference between the multiple reference input values to ADS131M08MET-EVM and the measured values, shown on the PC GUI. The reference input values to ADS131M08MET-EVM are generated by a PTS3.3C source generator meter or reference meter from MTE, while the measured values calculated by the Energy Library are reported in the PC GUI.
| VOLTAGE (V) | % ERROR Phase A | % ERROR Phase B | % ERROR Phase C |
|---|---|---|---|
| 270 | 0.00555 | 0.01444 | 0.02444 |
| 260 | 0.00384 | 0.01307 | 0.02461 |
| 240 | 0.00375 | 0.00500 | 0.0112 |
| 230 | 0.01086 | 0.00304 | 0.01652 |
| 220 | 0.00863 | 0.01090 | 0.00090 |
| 200 | 0.00700 | 0.00500 | 0.00650 |
| 180 | 0.01055 | 0.00111 | 0.00388 |
| 160 | 0.00250 | 0.00687 | 0.01874 |
| 140 | 0.00214 | 0.00428 | 0.00071 |
| 120 | 0.00666 | 0.01916 | 0.00999 |
| 100 | 0.00300 | 0.00900 | 0.00200 |
| 90 | 0.01300 | 0.00922 | 0.00988 |
| CURRENT (A) | % ERROR Phase A | % ERROR Phase B | % ERROR Phase C |
|---|---|---|---|
| 0.1 | 0.00399 | 0.04498 | 0.00499 |
| 0.25 | 0.02239 | 0.01159 | 0.00200 |
| 0.50 | 0.00179 | 0.01220 | 0.01940 |
| 1.00 | 0.01999 | 0.01499 | 0.00500 |
| 2.00 | 0.01649 | 0.00449 | 0.00699 |
| 5.00 | 0.00539 | 0.01339 | 0.01139 |
| 10.00 | 0.00999 | 0.01000 | 0.00950 |
| 20.00 | 0.01449 | 0.01449 | 0.02570 |
| 30.00 | 0.03366 | 0.02666 | 0.02899 |
| 40.00 | 0.01124 | 0.02825 | 0.03625 |
| 50.00 | 0.01398 | 0.01019 | 0.01720 |
| 60.00 | 0.01566 | 0.01683 | 0.01166 |
| 70.00 | 0.00642 | 0.00414 | 0.01842 |
| 80.00 | 0.00749 | 0.00475 | 0.01062 |
| 90.00 | 0.02321 | 0.01988 | 0.00100 |
| 100.00 | 0.02099 | 0.03199 | 0.00120 |
| CURRENT (A) | AVG ERROR (%) PF = 1, cos ϕ = 0° | LIMIT (%) [CLASS 0.1] IEC 62053-22 (PF 1) | LIMIT (%) [CLASS 0.2] IEC 62053-22 (PF 1) | AVG ERROR (%) PF = 0.5i, cos ϕ = 60° | LIMIT (%) [CLASS 0.1] IEC 62053-22 (PF 0.5i|0.8c) | LIMIT (%) [CLASS 0.2] IEC 62053-22 (PF 0.5i|0.8c) | AVG ERROR (%) PF = 0.8c cos ϕ = –36.87° |
|---|---|---|---|---|---|---|---|
| 1.0 | 0.024 | ±0.2 | ±0.4 | ||||
| 1.5 | 0.013 | ±0.1 | ±0.2 | ||||
| 3 | 0.001 | ±0.1 | ±0.2 | 0.093 | 0.25 | 0.5 | -0.084 |
| 10 | 0.009 | ±0.1 | ±0.2 | ||||
| 15 | 0.005 | ±0.05 | ±0.1 | 0.040 | 0.15 | 0.3 | -0.055 |
| 30 | 0.009 | ±0.1 | ±0.2 | ||||
| 50 | 0.008 | ±0.1 | ±0.2 | –0.087 | 0.15 | 0.3 | -0.015 |
| 75 | 0.027 | ±0.1 | ±0.2 | ||||
| 90 | 0.047 | ±0.1 | ±0.2 | ||||
| 100 | 0.014 | ±0.1 | ±0.2 | –0.122 | 0.15 | 0.3 | 0.061 |
| VOLTAGE (V) | AVERAGE ERROR (%) | Test Current (A) |
|---|---|---|
| 90 | –2.062 | 0.05 |
| VOLTAGE (V) | TEST CURRENT (A) |
AVERAGE ERROR (%) |
LIMIT (%) [CLASS 0.1] |
LIMIT (%) [CLASS 0.2] |
|---|---|---|---|---|
| 120 | 1.5 | 0.075 | REF | REF |
| 108 | 1.5 | 0.072 | ±0.1 | ±0.2 |
| 235 | 1.5 | 0.074 | ±0.1 | ±0.2 |
| 270 | 1.5 | 0.071 | ±0.1 | ±0.2 |
| 297 | 1.5 | 0.069 | ±0.1 | ±0.2 |
| 120 | 15 | 0.053 | REF | REF |
| 108 | 15 | 0.053 | ±0.1 | ±0.2 |
| 235 | 15 | 0.055 | ±0.1 | ±0.2 |
| 270 | 15 | 0.052 | ±0.1 | ±0.2 |
| 297 | 15 | 0.052 | ±0.1 | ±0.2 |
| CIRCUIT | TEST CURRENT (A) | AVERAGE ERROR (%) | LIMIT (%) [CLASS 0.1] | LIMIT (%) [CLASS 0.2] |
|---|---|---|---|---|
| ABC | 1.5 | 0.048 | REF | REF |
| CBA | 1.5 | 0.041 | ±0.1 | ±0.3 |
| ABC | 15 | 0.026 | REF | REF |
| CBA | 15 | 0.018 | ±0.1 | ±0.3 |
| CIRCUIT | TEST CURRENT (A) |
AVERAGE ERROR (%) |
LIMIT(%) [CLASS 0.1] |
LIMIT (%) [CLASS 0.2] |
|---|---|---|---|---|
| All | 1.5 | 0.056 | REF | REF |
| Circuit A | 1.5 | 0.034 | ±0.15 | ±0.3 |
| Circuit B | 1.5 | 0.066 | ±0.15 | ±0.3 |
| Circuit C | 1.5 | 0.042 | ±0.15 | ±0.3 |
| All | 15 | 0.032 | REF | REF |
| Circuit A | 15 | 0.011 | ±0.15 | ±0.3 |
| Circuit B | 15 | 0.046 | ±0.15 | ±0.3 |
| Circuit C | 15 | 0.030 | ±0.15 | ±0.3 |