The following general guidelines are followed for
this evaluation module:
- Place decoupling capacitors close to the associated pins of the ADS131M08.
- Use ground planes instead of ground traces and minimize the cuts in the ground plane, especially near the ADS131M08.
- Keep the analog inputs of each ADC channel symmetrical and as close as possible to each other.
- For the ADS131M08 device, place the 0.1μF capacitor closest to the AVDD pin than the 1μF capacitor. Do the same thing also for the 0.1μF and 1μF capacitors connected to DVDD.
- Minimize the length of the traces used to connect the crystal to the microcontroller.
- Use wide traces for power-supply connections.