SBAU487 August 2025
Before running the ADS131M08MET-EVM GUI, plug the USB to RS-232 cable into the PC and verify the COM port used. On a Microsoft Windows PC, open the Device Manager and scroll down to Ports (COM and LPT). Find the Prolific PL2303GS USB Serial COM Port and note the port used. The COM ports being used are enclosed in parentheses as shown in Figure 3-1.
Open the folder on the PC that contains the metrology GUI. By default, the GUI is located in C:\ti\mspm0_sdk_(version)\tools\metrology_gui. Before running the calibrator.exe file, open and edit the calibration-config.xml file. Open the calibration-config.XML file with a text editor and search for <meter position="1">. The line following the meter position must use the same COM port that is associated with the PL2303GS COM port as shown in Figure 3-2. Be sure to save any changes before running the calibrator.exe file.