SBAU487 August 2025
When using Rogowski coils as the current sensor inputs, the shunt jumpers on JP1 through JP8 must be removed. Depending on the sensitivity of the coil, additional gain on the current input channels can be added as described in Section 2.7.3.
The MSPM0G1506 on the EVM is capable of performing software integration. To enable software integration, switch SW2 (see Figure 2-4) must be switched to the ON position followed by pressing the push-button switch SW4. TI reference design TIDA-010986 is an optional PCB design which incorporates hardware integration for up to three current inputs. The TIDA-010986 reference PCB can be plugged directly onto the ADS131M08MET-EVM through J9.