SBOK102 July 2025 INA1H94-SP
The INA1H94-SP was biased in a variety of different conditions for SEE testing, at both the recommended minimum and recommended maximum supply voltages. Midsupply or GND was used for both REFA and REFB. Current was monitored over time for both V+ and V-.
An example of three decapped units mounted on a characterization board is shown in Figure 4-3. Note that for SET testing, devices were powered in parallel and the test facility "stage" or backplane was moved between runs to target different DUTs. For SEL testing, only one device was connected at a time.
Figure 4-3 Characterization BoardAdditional correlation testing was performed on three units, each mounted on a simplified coupon board, using the device absolute maximum supply voltage (24V). Devices were exposed to a total fluence of 5 × 107 ions / cm2 (60krad of accumulated HDR TID), 2 × 107 ions / cm2 (24krad of accumulated HDR TID), and 1 × 107 ions / cm2 (12krad of accumulated HDR TID) respectively without any failures observed. This suggests the device has significant margin at the device recommended maximum operating voltage of 18V.