SBOK102 July 2025 INA1H94-SP
Studies were performed to characterize the effects of heavy-ion irradiation on the single-event latch-up (SEL) performance of the INA1H94-SP radiation-hardened, high common-mode voltage difference amplifier. For device qualification, heavy ions with an LETEFF of 75MeV-cm2 / mg were used to irradiate the devices with a fluence of 1 × 107 ions / cm2. The results demonstrated that the INA1H94-SP is SEL-free up to the specified surface LETEFF = 75MeV-cm2/ mg at 125°C.
Characterization of single-event transients (SET) and correlation testing of SEL were also performed, up to a surface LETEFF = 75MeV-cm2/ mg at 125°C.