SCDS461A November 2023 – January 2025 TMUX7348F-EP
PRODUCTION DATA
The following image shows a high level telemetry use case, where multiple sensors need to be monitored by the system. Here, multiple TMUX7348F-EP are used to expand the sensor count, and this scheme can be scaled up or down depending on the sensor count. If the board supply voltage is higher than the fault voltage supply (VFP or VFN) of the multiplexer, then the TMUX7348F-EP will disconnect the source input from passing the signal to protect the downstream ADC. The drain pin of the mux will be pulled up to the fault voltage supply voltage VFP through a 40 kΩ resistor to allow the ADC to determine a fault condition has occurred.