SDAA014 November 2025 AM2752-Q1 , AM2754-Q1
The following section details an example setup for a McASP where the bit clock and frame sync are configured as inputs.
| Description | GF MUX AUXCLK Source | AHCLK | Bit Clock | Frame Sync |
|---|---|---|---|---|
| McASP clock peripheral with an external AUXCLK reference | AUDIO_EXT_REFCLK<n> | Externally Generated | Externally Generated | Externally Generated |
In this example, the McASP is being configured for a 48 kHz frame sync and TDM8 frame format with 32-bit words resulting, in a bit clock frequency of 12.288 MHz. The GF MUX is configured to point to the external reference mux which is selecting AUDIO_EXT_REFCLK0 source that is 24.576 MHz from an external driver. The SDK driver sets the AHCLK and ACLK dividers but they are not used as ACLK and AFS is externally driven.
When the AHCLK is internally generated then the AHCLK can optionally be output on any of the AUDIO_EXT_REFCLK pins to provide a system clock reference output.
Additionally, the clock loss detection feature of the McASP is enabled with an internally generated AHCLK. For additional information on the clock loss detection for the McASP, refer to the Clock Failure Detection chapter within the MCASP Error Reporting section of the AM275x Technical Reference Manual.