SDAA132 December 2025 MSPM33C321A , MSPM33C321A-Q1
The MSPM33C comparator module (COMP) is an analog voltage comparator with general comparator functionality.
The COMP module includes internal and external inputs that can be used to flexibly to process analog signals. An internal temperature sensor can be used as a direct input to the COMP.
The MSPM33C Comparator module also combines two COMP to implement a window comparator function. As shown in Figure 6-3, COMP0 and COMP1 can be configured together to create a window comparator. In this configuration, the input signal is connected to the positive terminal of the comparators connected together, and the upper and lower threshold voltages are connected to the negative terminal of the comparators.
The COMP module also includes a SHORT switch that can be used to build a simple sample-and-hold for the comparator.
As shown in Figure 6-4, the required sampling time is proportional to the size of the sampling capacitor (CS), the resistance of the input switches in series with the short switch (R), and the resistance of the external source (RS). The sampling capacitor CS must be greater than 100pF. The time constant, Tau, to charge the sampling capacitor CS can be calculated with Equation 2.
Depending on the required accuracy, use 3 to 10 Tau as the sampling time. With 3 Tau, the sampling capacitor is charged to approximately 95% of the input signals voltage level. With 5 Tau, the sampling capacitor is charged to more than 99%, and with 10 Tau the sampled voltage is sufficient for 12-bit accuracy.