SDAA132 December 2025 MSPM33C321A , MSPM33C321A-Q1
The MSPM33C bootloader (BSL) is implemented on UART, I2C, and CAN serial interfaces. In MSPM33C devices, the BSL can automatically select the interface used to communicate with the device. The BSL communication pins are predefined in the ROM based bootloader. The specific instance of the peripheral interfaces that is used depends on the selected device and can be found in the device-specific data sheet. Refer to the device data sheet to find which pin has been assigned for BSL communication function before the hardware design.