SDAA170 September 2026 TPS61383-Q1
Properly setting the battery balancing current is important for optimizing the cell-balancing function. The balancing current magnitude is jointly determined by the on-chip NMOS FET and the resistance value of the input filter resistor. The recommended minimum value of the input filter resistors when using internal balancing is 20Ω. This results in a balancing current of approximately 35mA.