SLAAED5A June   2023  – September 2025 AFE11612-SEP , OPA4H199-SEP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. LDMOS and GaN Power Amplifier FET PA Basics
  5. VGS Compensation
  6. Sequencing
  7. An Integrated PA Biasing Solution
  8. Negative Biasing for GaN PAs
  9. Fast Switching for TDD Applications
  10. VDRAIN Switching Circuit
  11. Controlled Gate-Sequencing Circuit
  12. VDRAIN Monitoring
  13. 10External Negative Power Supply Monitoring
  14. 11PA Temperature Monitoring
  15. 12Summary
  16. 13References
  17. 14Revision History

Controlled Gate-Sequencing Circuit

There is importance to control the PA during start-up, shutdown, and alarm conditions, to make sure that the PA is not damaged during these events. This is accomplished by creating a three input logic AND gate of key signals: VREF, HOST PA_EN, and ALARM.

 PA_ON AND Gate Figure 8-1 PA_ON AND Gate

VREF is used as the device good signal for the PA_ON output. This makes sure that the PA never has the drain voltage applied at start-up, as the VREF must be enabled by the host controller after the AFE11612-SEP starts up. The ALARM signal from the AFE11612-SEP circuit can force the PA_ON to 0 V if the AFE11612-SEP detects any alarms. Finally, the host micro controller has the option of turning off PA_ON. Table 8-1 shows how all of the digital outputs interact with the PA_ON.

Table 8-1 PA_ON Truth Table
VREF PA_EN ALARM PA_ON
0V X X Low
X 0V X Low
X X 0V Low
2.5V High High High

Here is an example of the PA_ON power on sequence:

  1. The AFE11612-SEP is initialized. The host sends the command to turn on the VREF. With no alarm state at startup, the ALARM pin is High-Z. The host keeps PA_EN Low to keep the PA off.
  2. Next, the drain power is turned on. The host sets PA_EN High, enabling the PA_ON signal.
  3. Third, an alarm condition is shown. The ALARM goes to 0V, turning off the PA_ON and thus turning off the PA to protect the PA.
  4. Fourth, the alarm condition is cleared. ALARM returns to High-Z, and the PA_ON is on.
  5. Lastly, before the part powers off, disable PA_EN to turn off the PA_ON. Power down the AFE11612-SEP.
 PA_ON Power Sequence Control Figure 8-2 PA_ON Power Sequence Control