SLAAED5A June 2023 – September 2025 AFE11612-SEP , OPA4H199-SEP
IDS is dependent on the temperature of the PA. The IDS variations due to thermal drift create the need to compensate the PA by adjusting one of the other two variables in the system: VDRAIN or VGS. Although there are many reasons why adjusting VDRAIN is implemented in different RF applications, the response of the output power is minimal compared to the change in the VDRAIN voltage, as shown in Figure 1-2. Adjusting VGS allows for faster response time and total amplitude of the output power making it more practical for temperature compensation and other applications.
Figure 2-1 GaN PA VGS Bias Voltage vs Temperature to maintain constant IDSFigure 2-1 shows VGS needs to be adjusted to ensure a static IDS due to thermal drift. Applications utilizing these PAs require implementing this kind of compensation to ensure that the power of the antenna system is tightly controlled. VGS compensation can be implemented by either measuring the temperature of the PA, or measuring the IDS using a current shunt and adjusting the VGS accordingly.