SLAAER4 March 2025 AFE781H1 , AFE782H1 , AFE881H1 , AFE882H1 , DAC8740H , DAC8741H , DAC8742H
Below are some of the equipment needed to run HART testing for your field transmitter.
There are also a few specialized pieces of equipment required to run the HART physical layer tests. These devices are shown in Figure 3-1.
A HART test system is required for the HART protocol testing. While this system is mostly required for the data link layer and command tests, the test system can be used to generate the HART responses from the transmitter to view the specific FSK bits and responses. The HART test system is Linux® based, and runs tests with a set of commands designed by FieldComm. The HART test system requires two HART registered RS-232 modems.
The HCF_TOOL-31 filter is needed for the physical layer tests. This filter is a passband Butterworth filter that passes the HART FSK digital signal. The filter has a 2nd order roll-off below 500Hz, 1st order roll-off above 10kHz, and a passband gain of 10. This filter passes the HART FSK signal but removes the lower frequencies of the primary variable and any noise from higher frequencies.
The HCF_TOOL-32 filter is also required. This filter is a low-pass Butterworth filter with a 2nd order roll-off above 25Hz and a passband gain of 10. This low-pass filter passes the analog primary variable from a field transmitter and rejects the HART FSK signal and higher frequencies.
Finally, the FSK Physical Layer Test interface is used to increase and decrease the HART sinusoids from the HART test system in the transmission. This device is used to determine the sensitivity of the field transmitter for detecting the HART signal.
The HART test system, the HCF_TOOL-31 filter, the HCF_TOOL-32 filter, and the FSK Physical Layer Test interface can be purchased from FieldComm.