SLAAER4 March 2025 AFE781H1 , AFE782H1 , AFE881H1 , AFE882H1 , DAC8740H , DAC8741H , DAC8742H
Previously, Figure 2-1 showed the block diagram of the AFE882H1 device. In the middle of the figure is the HART communication protocol logo. The logo indicates the device was designed into a transmitter in a HART-registered product.
To be HART registered, the device is first tested by the company that created the device. Test results are used to generate a report sent to the FieldComm Group with an application for registration. Test results include physical layer tests that verify the waveform, check the timing of the HART FSK carrier signal, and verify timing with some HART specific digital lines built into the HART modem. Additionally, there are many tests that verify the HART protocol to check that the device has the proper response to commands from a HART controller.