The HART physical layer tests are
described in HCF TEST-2. This document defines the requirements for testing HART devices
for compliance with the HART FSK Physical Layer Specification. These tests verify many
different parameters of the HART communication.
- Verify the bit rate and signal
frequencies for the HART transmission.
- Verify that a carrier detect signal is sent within a minimum
time after the start or stop of a HART transmission.
- Measure the low-pass primary variable
signal to check that a carrier detect start or stop does not disrupt the
transmission of the primary variable.
- Check that the output noise is below a maximum level when the
HART is not transmitting.
- Testing HART communications while cycling the primary variable between the
minimum of 4mA and maximum of 20mA (analog rate of change test).
- Measure the HART device to verify
high receive impedance over the frequency of the primary variable and HART frequency
band.
- Test HART transmission in the
presence of in-band and out-of-band sinusoidal noise.
- Check the carrier detect level to
make sure a HART signal is detected when the signal is at the minimum amplitude, and
not detected below a lower amplitude, while maintaining carrier detect timing.
As part of the physical layer of the HART
protocol, these tests cover the timing and amplitude of the HART signal as generated by
the AFE882H1 and with the surrounding circuitry. The following sections describe the
HART physical layer tests and test setups.