SLAAER4 March 2025 AFE781H1 , AFE782H1 , AFE881H1 , AFE882H1 , DAC8740H , DAC8741H , DAC8742H
Figure 3-2 shows a block diagram of the HART FSK sinusoid test. Most HART tests require a similar setup with the transmitter as the device under test. The FSK sinusoid test verifies that the HART signal have the correct frequencies and wave shape for transmission.
A Keysight E36313A is used as the 24V power supply. The power supply powers the loop and the transmitter sets the current through the loop. A series resistor is used to measure the current through the loop, but also attaches to the HART test system through a modem.
For the HART FSK sinusoid test, an oscilloscope measures the HART transmitted signals. The HART tester sends commands and the oscilloscope plots the responses to find a series of 1s and 0s to measure the HART bits. A frequency counter can be used to measure the frequency of the FSK bits, but an oscilloscope can also be used to verify the timing.
Figure 3-3 and Figure 3-4 define the tolerance of the HART FSK signals. As previously mentioned, the two FSK signals are 1200Hz and 2200Hz. However, there is some acceptable variation in the signal.
These measurements define the FSK frequency variation allowed, the minimum and maximum voltages, and the rise times needed for the HART signal. In addition to the waveform requirements the two FSK frequencies, there is a transition requirement for the waveform shown in Figure 3-5.
These diagrams show the tolerance for amplitude of the HART signal, the frequency variation, and the rise time of the signals. To pass the tests, the HART sinusoid must fit within these trapezoidal windows shown in the figures.
The waveforms are taken from the AFE882H1 transmitter test setup using an oscilloscope. Figure 3-6 shows the oscilloscope photos taken for the two HART FSK sinusoids and Table 3-1 shows the test data taken from the measurements.
| FSK FREQUENCY | TEST | MEASURED | MINIMUM | MAXIMUM | RESULT |
|---|---|---|---|---|---|
| 1200Hz | Frequency | 1201Hz | 1188Hz | 1212Hz | Pass |
| Amplitude | 458mVPP | 400mVPP | 600mVPP | Pass | |
| Waveform rise time | 130µs | 80µs | 200µs | Pass | |
| Waveform fall time | 130µs | 80µs | 200µs | Pass | |
| 2200Hz | Frequency | 2202Hz | 2178Hz | 2222Hz | Pass |
| Amplitude | 478mVPP | 400mVPP | 600mVPP | Pass | |
| Waveform rise time | 80µs | 75µs | 200µs | Pass | |
| Waveform fall time | 80µs | 75µs | 200µs | Pass |
While a 250Ω resistor is commonly used in 4-20mA loops, a 500Ω current sense resistor is required for this and the other physical layer tests.