SLASF43A December 2023 – September 2026 AFE782H1 , AFE882H1
PRODUCTION DATA
Connections of the HART signal to the loop are done through the AFE882H1 MOD_OUT and RX_IN pins. Similar to converting the VOUT pin voltage to the loop current magnitude, the HART output from the MOD_OUT pin is converted from a voltage to a current. A dc-blocking capacitor of 1000pF is used to couple in the HART signal, without the dc output offset from the MOD_OUT pin. From MOD_OUT, the HART sinusoid nominal output is 500mVPP. Equation 15 shows that this VMOD HART sinusoid voltage is set across a 499kΩ resistor to create signal voltage VLOOPAC superimposed onto VLOOP–.
The VLOOP_AC voltage sets the HART-modulated loop current that flows from ground to LOOP– through the 20Ω resistor. This current is sourced from ground but controlled by the current sunk from Q4 coming from the start-up circuit. Equation 16 calculates the total loop current based on the 20mVPP of VLOOP_AC.
Using the 1000pF capacitor as a dc-blocking capacitor and the 499kΩ resistor, the 500mVPP MOD_OUT signal is converted to a 1mAPP HART signal on the current loop.
HART signals are received by the AFE882H1 through the RX_IN pin. A dc-blocking capacitor for the HART input at RX_IN is shown with a series resistance of 1kΩ in Figure 8-2. A diode clamps the pin to the device supply and the resistance limits the input current. This configuration protects the RX_IN from damage from an overvoltage event at the start up of the circuit.