SLASF43A December 2023 – September 2026 AFE782H1 , AFE882H1
PRODUCTION DATA
Figure 8-3 shows a block diagram of a loop-powered, 4mA to 20mA current transmitter.
The terminals connected to the loop are shown on the right side of the block diagram. This connection to the loop powers the entire transmitter. A bridge rectifier at the input protects against reverse connection to the loop. The rectified loop voltage powers a start-up circuit that provides power to an LDO, that in turn powers the AFE882H1 and an MCU.
The AFE882H1 controls the loop current through the voltage-to-current (V-to-I) converter block. The DAC voltage sets the output from 0V to 2.5V. The output is sent through a V-to-I converter block using an OPA333 and an NPN bipolar junction transistor (BJT).
The HART signal is not received at the positive terminal of the 4mA to 20mA connections, but instead is received after the loop-protection rectifier. This HART signal input is capacitively coupled to this LOOP+ internal node of the circuit as shown in Figure 8-2. The HART signal output is modulated onto the loop current from the AFE882H1 through the V-to-I converter circuit.