SLAU144K December 2004 – August 2022 MSP430AFE221 , MSP430AFE222 , MSP430AFE223 , MSP430AFE231 , MSP430AFE232 , MSP430AFE233 , MSP430AFE251 , MSP430AFE252 , MSP430AFE253 , MSP430F2001 , MSP430F2002 , MSP430F2003 , MSP430F2011 , MSP430F2012 , MSP430F2013 , MSP430F2101 , MSP430F2111 , MSP430F2112 , MSP430F2121 , MSP430F2122 , MSP430F2131 , MSP430F2132 , MSP430F2132-EP , MSP430F2232 , MSP430F2234 , MSP430F2252 , MSP430F2252-Q1 , MSP430F2254 , MSP430F2272 , MSP430F2272-Q1 , MSP430F2274 , MSP430F2274-EP , MSP430F233 , MSP430F2330 , MSP430F235 , MSP430F2350 , MSP430F2370 , MSP430F2410 , MSP430F2416 , MSP430F2417 , MSP430F2418 , MSP430F2419 , MSP430F247 , MSP430F2471 , MSP430F248 , MSP430F2481 , MSP430F249 , MSP430F2491 , MSP430F2616 , MSP430F2617 , MSP430F2618 , MSP430F2619 , MSP430G2001 , MSP430G2101 , MSP430G2102 , MSP430G2111 , MSP430G2112 , MSP430G2121 , MSP430G2131 , MSP430G2132 , MSP430G2152 , MSP430G2153 , MSP430G2201 , MSP430G2201-Q1 , MSP430G2202 , MSP430G2203 , MSP430G2210 , MSP430G2211 , MSP430G2212 , MSP430G2213 , MSP430G2221 , MSP430G2230 , MSP430G2231 , MSP430G2231-Q1 , MSP430G2232 , MSP430G2233 , MSP430G2252 , MSP430G2253 , MSP430G2302 , MSP430G2303 , MSP430G2312 , MSP430G2313 , MSP430G2332 , MSP430G2333 , MSP430G2352 , MSP430G2353 , MSP430G2402 , MSP430G2403 , MSP430G2412 , MSP430G2413 , MSP430G2432 , MSP430G2433 , MSP430G2444 , MSP430G2452 , MSP430G2453 , MSP430G2513 , MSP430G2533 , MSP430G2544 , MSP430G2553 , MSP430G2744 , MSP430G2755 , MSP430G2855 , MSP430G2955 , MSP430TCH5E
| * DECD[.W] | Double-decrement destination | |
| * DECD.B | Double-decrement destination | |
| Syntax |
DECD dst
or
DECD.W dst | |
DECD.B dst | ||
| Operation | dst – 2 → dst | |
| Emulation |
SUB #2,dst | |
SUB.B #2,dst | ||
| Description | The destination operand is decremented by two. The original contents are lost. | |
| Status Bits | N: | Set if result is negative, reset if positive |
| Z: | Set if dst contained 2, reset otherwise | |
| C: | Reset if dst contained 0 or 1, set otherwise | |
| V: | Set if an arithmetic overflow occurs, otherwise reset | |
| Set if initial value of destination was 08001 or 08000h, otherwise reset | ||
| Set if initial value of destination was 081 or 080h, otherwise reset | ||
| Mode Bits | OSCOFF, CPUOFF, and GIE are not affected. | |
| Example | R10 is decremented by 2. | |
DECD R10 ; Decrement R10 by two
; Move a block of 255 bytes from memory location starting with EDE to
; memory location starting with TONI.
; Tables should not overlap: start of destination address TONI must not
; be within the range EDE to EDE+0FEh
MOV #EDE,R6
MOV #255,R10
L$1 MOV.B @R6+,TONI-EDE-2(R6)
DECD R10
JNZ L$1| Example | Memory at location LEO is decremented by two. | |
DECD.B LEO ; Decrement MEM(LEO)| Decrement status byte STATUS by two | ||
DECD.B STATUS