SLAU957 June 2025
Run Script file:To run a script file, first select the file in the Scripts window, and then press F5 (or select Run and then Buffer in the menu bar).
Run part of script: To run part of a script file, select the lines in the Editor window, and then press F7 (or select Run and then Run Selection in the menu bar).
Stop Execution: To stop the current execution, press F10 (or select Run and then Stop in the menu bar).
Clear Session: To clear the current session and reset the Latte GUI to the initial state, press Ctrl+T (or select Session and then Clear Session in the menu bar). This process is equivalent to a restart and is used to restart a session without closing the GUI.