SLUS812E February 2008 – September 2025 TPS51200
PRODUCTION DATA
During TPS51200 tracking start-up, the REFIN voltage follows the rise of the VDDQ rail through a voltage divider, and REFOUT (VREF) follows REFIN once the REFIN voltage is greater than 0.39V. When the REFIN voltage is lower than 0.39V, VREF is 0V.
The JEDEC DDR2 SDRAM Standard (JESD79-2E) states that VREF must track VDDQ/2 within ±0.3V accuracy during the start-up period. To allow the TPS51200
device to meet the JEDEC DDR2 specification, a resistor divider can be used to provide the VREF signal to the DIMM. The resistor divider ratio is 0.5 to ensure that the VREF voltage equals VDDQ/2.
Figure 6-5 Resistor Divider CircuitWhen selecting the resistor value, consider the impact of the leakage current from the DIMM VREF pin on the reference voltage. Use Equation 4 to calculate resistor values.

where
Consider the MT47H64M16 DDR2 SDRAM component from Micron as an example. The MT47H64M16 datasheet shows the maximum VREF leakage current of each DIMM is ±2µA, and VREF(DC) variation must be within ±1% of VDDQ. In this DDR2 application, the VDDQ voltage is 1.8V. Assuming one TPS51200 device needs to power 4 DIMMs, the maximum total VREF leakage current is ±8µA. Based on the calculations, the resistor value should be lower than 4.5kΩ. To ensure sufficient margin, 100Ω is the suggested resistor value. With two 100Ω resistors, the maximum VREF variation is 0.4mV, and the power loss on each resistor is 8.1mW.