SLUSF91 December 2025 UCC23710
PRODUCTION DATA
The input stage of UCC23710 integrates a diode emulator(e-diode) interfacing through its Anode and Cathode. When the e-diode is forward biased by applying a positive voltage to the Anode with respect to the Cathode, a forward current IF flows into the e-diode. The forward voltage drop across the e-diode is 1.7V (typ). An external resistor on the Anode should be used to limit the forward current. When IF exceeds the threshold current IFLH (1mA typ.), a high frequency signal is transmitted across the isolation barrier that is then detected by the receiver and VOUT is driven high. The dynamic impedance of the e-diode is very small(<1.0Ω) and the temperature coefficient of the e-diode forward voltage drop is 0.7mV/°C typically. This leads to excellent stability of the forward current IF across all operating conditions. If the Anode voltage drops below VF_HL (0.8V), or reverse biased, the gate driver output is driven low.The recommended range for the forward current is 5mA to 20mA.
The reverse breakdown voltage of the e-diode is ~6V . For normal operation, a reverse bias of up to 5V is allowed. The large reverse breakdown voltage of the e-diode enables UCC23710 to be operated in interlock architecture. The system designer has the flexibility to choose a 3.3V or 5.0V signal source to drive the input stage of UCC23710 using an appropriate input resistor. Interlock architecture prevents both the e-diodes from being "ON" at the same time, preventing shoot through in the IGBTs. It also ensures that if both PWM signals are erroneously stuck high (or low) simultaneously, both gate driver outputs will be driven low.
For best noise immunity performance, it is recommended to place the current limiting resistor connected to the anode. Cathode should be connected directly to ground.