SLVA275C january 2010 – may 2023 UCD9081
The GpDir field in the configuration parameters specifies the direction (input or output) of RAILn or GPOn. This should correspond with the desired enable settings. If a RAIL or GPO is enabled, it should also be set as an output. The register contents are as follows:
| Address | Size | Default Value | Description |
| 0xE048 | 2 | 0xFFFF | Input / Output parameters for GPOn and RAILn |
The format of the register is as follows:
| RAILn or GPOn | Meaning |
|---|---|
| 0 | Set the RAILn or GPOn to output (enable) |
| 1 | Set the RAILn or GPOn to input (disable) |