SLVA275C january 2010 – may 2023 UCD9081
The DependencyMasks field in the configuration parameters defines the rail dependency masks used for rail and GPO shutdown. This mask represents the set of other rails and GPOs that must be shut down when this rail shuts down. Note that because only rails are monitored, the table only has entries for the shutdown of rails. In the dependency mask itself, there are bits that allow for GPO shutdown.
The address map for these registers is as follows:
| Address | Size | Default Value | Description |
|---|---|---|---|
| 0xE100 | 2 | 0x007F | Dependency mask for rail 1 |
| 0xE102 | 2 | 0x0001 | Dependency mask for rail 2 |
| 0xE104 | 2 | 0x0002 | Dependency mask for rail 3 |
| 0xE106 | 2 | 0x0004 | Dependency mask for rail 4 |
| 0xE108 | 2 | 0x0008 | Dependency mask for rail 5 |
| 0xE10A | 2 | 0x0010 | Dependency mask for rail 6 |
| 0xE10C | 2 | 0x0020 | Dependency mask for rail 7 |
| 0xE10E | 2 | 0x0040 | Dependency mask for rail 8 |
The format for each register is as follows: