SLVA275C january 2010 – may 2023 UCD9081
The OutOfRegulationWidth field in the configuration parameters specifies the maximum amount of time that the rail is allowed to be out of regulation before an error is declared (glitch duration). The address map for these registers is as follows:
| Address | Size | Default Value | Description |
|---|---|---|---|
| 0xE140 | 2 | 0x0010 | The out-of-regulation duration permissible without flagging error for rail 1 |
| 0xE142 | 2 | 0x0010 | The out-of-regulation duration permissible without flagging error for rail 2 |
| 0xE144 | 2 | 0x0010 | The out-of-regulation duration permissible without flagging error for rail 3 |
| 0xE146 | 2 | 0x0010 | The out-of-regulation duration permissible without flagging error for rail 4 |
| 0xE148 | 2 | 0x0010 | The out-of-regulation duration permissible without flagging error for rail 5 |
| 0xE14A | 2 | 0x0010 | The out-of-regulation duration permissible without flagging error for rail 6 |
| 0xE14C | 2 | 0x0010 | The out-of-regulation duration permissible without flagging error for rail 7 |
| 0xE14E | 2 | 0x0010 | The out-of-regulation duration permissible without flagging error for rail 8 |
The contents of this register are as follows: