SLVA275C january 2010 – may 2023 UCD9081
The SeqEventPending field in the configuration parameters determines if the RAILn or GPOn will be enabled or disabled for sequencing. These values should align with SequenceEventParameter (see Section 4.2.4), if RAILn/GPOn is not disabled, it should also not be disabled in these parameters.
| Address | Size | Default Value | Description |
|---|---|---|---|
| 0xE068 | 2 | 0x0000 | Sequencing parameters for GPOn and RAILn |
The format of the register is as follows:
| RAILn or GPOn | Meaning |
| 0 | Disable sequencing on RAILn or GPOn |
| 1 | Enable sequencing on RAILn or GPOn |