SLVAF66 June   2021 DRV3255-Q1 , DRV8300 , DRV8301 , DRV8302 , DRV8303 , DRV8304 , DRV8305 , DRV8305-Q1 , DRV8306 , DRV8307 , DRV8308 , DRV8320 , DRV8320R , DRV8323 , DRV8323R , DRV8340-Q1 , DRV8343-Q1 , DRV8350 , DRV8350F , DRV8350R , DRV8353 , DRV8353F , DRV8353R

 

  1. 1 Introduction to High-Power Motor Applications
    1. 1.1 Effects of a Poorly-Designed High-Power Motor Driver System
    2. 1.2 Example of the High-Power Design Process
  2. 2 Examining a High-Power Motor Drive System at a High Level
    1. 2.1 Anatomy of the Motor Drive Power Stage and How to Troubleshoot
    2. 2.2 Troubleshooting a High-Power System
  3. 3 High-Power Design Through MOSFETs and MOSFET Gate Current (IDRIVE)
    1. 3.1 MOSFET Gate Current
      1. 3.1.1 How Gate Current Causes Damage
      2. 3.1.2 Gate Resistors and Smart Gate Drive Technology
        1. 3.1.2.1 Gate Resistors
        2. 3.1.2.2 Smart Gate Drive and Internally-Controlled Sink and Source Gate Currents
        3. 3.1.2.3 Summary for Gate Resistors and Smart Gate Drive Technology
      3. 3.1.3 Example Gate Current Calculation for a Given FET
  4. 4 High-Power Design Through External Components
    1. 4.1 Bulk and Decoupling Capacitors
      1. 4.1.1 Note on Capacitor Voltage Ratings
    2. 4.2 RC Snubber Circuits
    3. 4.3 High-Side Drain to Low-Side Source Capacitor
    4. 4.4 Gate-to-GND Diodes
  5. 5 High-Power Design Through a Parallel MOSFET Power Stage
  6. 6 High-Power Design Through Protection
    1. 6.1 VDS and VGS Monitoring
      1. 6.1.1 Turning Off the FETs During an Overcurrent, Shoot-Through, or FET Shorting Event
    2. 6.2 Passive Gate-to-Source Pulldown Resistors
    3. 6.3 Power Supply Reverse Polarity or Power Supply Cutoff Protection
  7. 7 High-Power Design Through Motor Control Methods
    1. 7.1 Brake versus Coast
      1. 7.1.1 Algorithm-Based Solutions
      2. 7.1.2 External Circuit Solutions
      3. 7.1.3 Summary of Brake versus Coast
  8. 8 High-Power Design Through Layout
    1. 8.1 What is a Kelvin Connection?
    2. 8.2 General Layout Advice
  9. 9 Conclusion
  10. 10Acknowledgments

Example Gate Current Calculation for a Given FET

For this example, the DRV835x family of devices is used and paired with the CSD19536KTT power MOSFETs, which are used in the 54-V, 1.5-kW, > 99% efficient, 70 × 69 mm2 power stage reference design for 3-phase BLDC motors: TIDA-010056.

The steps for estimating the approximate gate current generally are:

  1. Find the FET part number and the associated data sheet
  2. Locate the Qgdvalue in the data sheet
  3. The typical Qgd is acceptable but always be aware of the minimum or maximum tolerance of the Qgd
  4. Estimate needed VDS rise and fall time. For many high-power systems, rise and fall times between 100 ns to 300 ns are a good starting point as a general guideline.
  5. Alternatively, the designer can rearrange Equation 2 to get the equation in terms of gate drive current (IDRIVE) instead of VDS slew rate (SRDS) where 25 V/µs to 100 V/µs is acceptable as general input:
Equation 2. I D R I V E =   Q g d t R i s e F a l l

Where:

  • IDRIVE = current sourced to or sunk out of the gate, in amps
  • tRiseFall = equivalent rise or fall time for the VDS (not VGS), in seconds
  • Qgd = inherent gate-to-drain charge of the MOSFET, in coulombs

For the case of the CSD19536KTT, Qgd = 17 nC and we can use the general guidelines to put 100 ns into the rise and fall time of Equation 3. Note, some designers like to make the fall time two times faster than the rise time.

Equation 3. I D R I V E =   17 × 10 - 9 100 × 10 - 9
Equation 4. I D R I V E =   170   m A

The DRV835x family does not have an IDRIVE setting of exactly 170 mA, but it does have lower options of 150 mA or 100 mA for source current and 100 mA for sink current. Source refers to the current taken from the gate voltage supply and pushed into the FET, which corresponds with the rise time; and sink refers to the rate at which charge is pulled from the gate of the FET and pushed to the source of the FET, which corresponds with the fall time.

In the case where the rise and fall time is 300 ns, the same equation can be used:

Equation 5. I D R I V E =   17 × 10 - 9 300 × 10 - 9
Equation 6. I D R I V E =   56   m A

Using the DRV835x family again, choose 50 mA for the source current but the smallest sink current is 100 mA. This is a perfect example for replacing the 0-Ω gate resistor with a nonzero value to get the equivalent gate sink current below the lowest setting. If not planning to have the 0-Ω gate resistor, traces must be cut and the board redesigned to get the desired performance.

Remember, we are merely using a starting gate drive current that was calculated with a safe general guideline. This is a first order equation and does not exactly match what is seen in the real system, but the goal is to get within a reasonable starting point. This is why we round down if the device does not have an exact selection, to make the equivalent rise or fall time to be longer than the calculated value. Designers are expected to increase or decrease this number after testing.