SLVSDM4F November 2018 – October 2026 TPS1HA08-Q1
PRODUCTION DATA
Figure 9-4 shows the behavior of the TPS1HA08-Q1 in this application when the MCU provides an enable pulse to beginning heating the resistive element. Shortly after the EN pin goes high, the load current begins to flow and the SNS pin measures the output current.
Figure 9-4 Heater Turn-on TimeBy measuring the voltage on the SNS pin, the TPS1HA08-Q1 can communicate back to the system MCU what the load current is. Figure 9-5 shows that when the seat heater approaches full load and IOUT jumps from a low load current of 1A up to a 5A load current, the load step is mirrored on the SNS pin.
Figure 9-5 SNS Response During Heater Load StepOne common concern in these type of applications is that the heating element can accidentally lose connection, creating an open load situation. In this case, it is designed for the TPS1HA08-Q1 to recognize that the load has been removed and report a FLT to the MCU. Figure 9-6 shows the behavior of the TPS1HA08-Q1 when there is no load attached. As soon as the DIAG_EN pin is engaged, the SNS output goes high and the ST output engages low. By monitoring these pins, the MCU can recognize there is a fault and notify the user that maintenance is required.
Figure 9-6 Open Load Detection If Heating Element is MissingImportantly, the TPS1HA08-Q1 also protects the system in the event of a short-circuit. Figure 9-7 shows the behavior of the device if it is enabled into a short circuit condition. If this is using the device option C, the current is clamped to the current limit ICL until it hits an over temperature event, at which point it shuts down. In this way, the system is protected from unchecked overcurrent in the event of a short circuit.
Figure 9-7 Overcurrent Behavior During Short Circuit Event